A guide to cord grips
The purpose of strain-relief cord grips
Cord grips, also called cable glands, perform a number of essential roles in cable management. Designed to attach and secure the end of an electric cable and the device it’s connected to, cord grips provide earthing, grounding, insulation, bonding and strain relief. They can also be used to seal cables which pass through bulkheads of gland plates.
They are often located in hazardous or harsh environments where they need to contain electrical sparks or flames, or repel outside contaminants such as dust, dirt and fluids, such as the challenges facing an outdoor utility cabinet. In addition to this, their job is to stop cables becoming twisted or pulled to ensure a secure connection and continual performance.
In our guide, we'll cover:
- How to choose cord grips
- The purpose of armoring in cables
- Types of cord grips
- Cord Grip Materials
- Installing cord grips
- Cord Grip Considerations
https://iec.ch/homepageHow to choose cord grips
You have a world of choices before you and unfortunately, there is no one-size-fits-all option. But it does mean that you can custom select a cord grip based on your parameters. And to do that, you first need to consider a range of environmental and application factors.
The role of the environment
It doesn’t matter whether you’re working in aerospace, industrial, marine, power and utility, telecommunications or any other key industry. What’s important is identifying the core application environment of your cord grip. Questions to ask yourself:
- Are you using it indoors or outdoors?
- Will it be situated in a safe industrial zone or a hazardous or explosive environment?
- What’s the temperature and is it constant?
- Is the surrounding area damp or dusty?
- Are there any gases or corrosive materials nearby?
Your answers will help determine the cord grip specs and whether it requires a special protective plating or coating.
The purpose of armoring in cables
Different cables demand different types of cord grips. For example, the requirements for an armored cable, also called steel wired armored (SWA) are different to those of unarmored cables. Armored, or SWA, cables are used on exterior walls or underground.
|
Type |
Characteristics |
Application |
| Armored | Extra layer of protection to prevent damage This may be a single wire armor, braided armor, pliable wire armor or double steel tape armor |
Areas where exposed to threat of mechanical damage |
| Unarmored | More basic than armored Can have no seal, or have a single outer seal or a double outer seal |
Fixed installations not exposed to risk of mechanical damage |
Does armored cable need conduit?
Typically, no. They’re armored for protection. You should use conduit for unarmored cable, however.
IP-rated cable glands
Cord grips are designed with safety in mind, so they come with an IP rating to ensure you know what you’re getting. The Ingress Protection Marking (IP) rates the glands depending on their design and efficiency throughout different tasks. These ratings often go up to IP68 and IP69K. It’s important to check that any devices placed in explosive atmospheres comply with national or international codes of practice. You can learn more about the ratings with IP codes and what they mean.
Types of cord grips
Below are examples of cord grips:
Spiral cord grips
These types of cord grips provide excellent strain relief to protect against conductor fatigue caused by flexing cables. IP68 rated, resisting dust, dirt and sand, and withstanding submersion in water for 30 minutes.
Rated IP68 for outstanding protection against the elements. Designed for superior sealing and strain relief, these cord grips are rated IP68 for excellent protection against the environment. With an IP68 rating, these are waterproof cable glands.
Right-angle design enables easy routing of wires in tight spaces. Liquid tight, with an IP68 rating. Suitable for outdoor enclosures. Made of durable nylon 6/6.
Cable gland size guide
- Cable diameter
- Construction size
- Cable material
For armored cables, you also need to consider:
- The diameter of the inner bedding
- The diameter of the lead covering
- The short circuit fault rating of the cable armor
- The type and size of the armor braid
Cord Grip Materials
Cable gland materials perform differently depending on the application, environment and cable type.
Metal cord grips are used in a range of applications, including the chemical industry, technology and areas with high demands on special mechanical and chemical stability. The pros are durability over time, even in wet conditions, and its rigid stability.
Plastic cord grips have a wide cable range due to their claw and seal design, which makes them extremely adaptable to various applications. The pros are resistance to salt water, grease and weak acids, just to name a few.
At a glance:
|
Material |
Common applications |
Characteristics |
| Metal cord grips |
|
|
| Nylon cord grips |
|
|
How to install a cable gland
Cable gland installation depends on the type of gland you’re using, but the basics are the same. You’ll need to follow the relevant codes of practice, your local regulations and the manufacturer’s cable-gland-installation instructions. Installation should only be carried out by a skilled person with experience and knowledge of cable glands.
Note: Take care not to damage loose entry wires.
Getting started
Step 1: Turn off all electrical equipment and disconnect any live wires
Step 2: Make sure your cord grip is compatible with your cables
Step 3: Keep cord grips clear of solvents, chemical substances, and dirt during installation
Installing cord grips
Step 1: Open the cable gland and remove the nut.
Step 2: Peel back the outer sheath of the cable to the same length of the cord grip itself. If there’s an inner metal armor, expose it.
Step 3: Insert the right end of the gland into the cable.
Step 4: Lay the peeled sheath or armor evenly around the gland.
Step 5: Apply the nut, taking care to tighten with a spanner to secure the gland in place.
Extra protection features
Your application or environment may demand the cord grip to possess a specific quality, above and beyond its basic function. That’s where you may consider one the following special features:
- Fire-stop cord grip which can withstand fire propagation through a barrier
- Explosion-proof cord grips
- EMI and RFI shielding and associated grounding features to minimize or eliminate electromagnetic or radio frequency interference
- Romex connections to specifically deal romex cables
- Wire mesh for additional strain relief
- Liquid tight cord grips to protect against penetrating oils and waters
Cord Grip Considerations
There are a few important considerations that fall outside of the categories above. So before you choose a cable gland, also ask yourself:
- Is the wire hole diameter large enough to house all the cables in the system?
- Is the cable diameter sufficient?
- Is the pressure rating high enough for your application needs?
- Is the mounting hold diameter large enough for my cord grip?
- Is the depth and size of the grip thread metric or PG?
- Is there a requirement for stopper plugs to close off any unused cable entries?
Download free CADs and try before you buy
Free CADs are available for most solutions, which you can download. You can also request free samples to ensure the solution you’ve chosen is exactly what you need. You might also find these guides helpful:
- Ultimate guide to cable management
- Quick guide: industrial components for outdoor cabinets
- Quick guide: the small HVAC components for your HVAC design
- Guide to cable strain relief and protection
If you’re not quite sure which cord grip will work best for your application, our experts are always happy to advise you, whether it’s with standard cable gland sizes, suitable outdoor cable glands or anything else that you need. We also offer plastic grommets, so we can help you with that too. Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.
Questions?
Email us at sales@essentracomponents.com or speak to one of our experts for further information on the ideal solution for your application 800-847-0486.