304 vs. 430 stainless steel: what’s the difference?
Stainless steels vary in their elemental and chemical composition. They share many of the same characteristics, but their individual properties set them apart from each other. We’ve put together this guide to help you understand not only how these two grades are similar, but also how they differ. We’ll cover:
What is 304 stainless steel?
Stainless steel grade 304 belongs to the austenitic stainless steels. It contains a minimum of 18% chromium and 8% – 10.5% nickel with a maximum of 0.08% carbon.
Chromium is the key element here – and it’s where stainless steel’s superior corrosion resistance comes from. The chromium forms a passive oxide layer on the surface of the steel, protecting it from rust and corrosion. The higher the chromium content, the greater the resistance to corrosion. Chromium also enhances the steel’s toughness and ductility, making it easy to work with. It’s also why 304 stainless steel stands up to high temperatures.
Nickel increases its resistance to corrosion, especially against acidic environments. The material's toughness and ductility is also helped by nickel, making it easier to form and fabricate. Carbon is added to improve the steel’s strength and hardness. However, if the carbon content is too high, it reduces the material's resistance to corrosion and makes it more difficult to weld.
304 stainless steel also contains small amounts of manganese, silicon, and sometimes molybdenum. These elements all contribute to the material's strength, formability, and weldability.
304 stainless steel is non-magnetic, which makes it useful in applications where magnetism is undesirable. This comes down to its austenitic microstructure, which is a face-centred cubic (FCC) crystal structure. The atoms in the lattice structure are symmetrically arranged, and their magnetic moments cancel each other out.
You can learn more in our guide, Understanding stainless-steel grades.
What is 304 stainless steel used for?
This corrosion-resistant metal is commonly used in these applications:
| Industry | Typical applications | Why |
|---|---|---|
| Food processing equipment | Tanks, pipes and containers | Resistance to corrosion, easy to clean |
| Consumer appliances | Sinks, refrigerators, dishwashers | Durability, resistance to corrosion, aesthetic appeal |
| Automotive | Exhaust systems, trim and grilles | Resistance to corrosion, aesthetic appeal |
| Medical equipment | Surgical instruments, dental instruments and implants | Biocompatibility, resistance to corrosion and withstands high-temperature cleaning processes |
| Chemical processing equipment | Reactors, tanks and pipelines | Resistance to corrosion, stands up to a range of chemicals |
| Aerospace components | Aircraft structures, engines | High strength-to-weight ratio, resistance to corrosion, thermal stability |
304 stainless steel is also used in small components. Examples include:
- Band, housing and screw are 304
- Mesh is 304
Properties of 304 stainless steel
The characteristics of 304 stainless steel – as with any material – are a result of its properties. Let’s take a closer look:
What is 430 stainless steel?
Explaining this stainless steel grade is easier when we consider 304 vs. 430 stainless steel differences. First, 430 belongs to the ferritic stainless steel grades with 17% chromium. Grade 304 has slightly higher chromium content with a minimum of 18%.
Grade 430 also lacks nickel. This makes 430 stainless steel not as strong for corrosion and chemical resistance in harsh environments when compared to 304 stainless steel. Mind you, grade 430 still has very good corrosion resistance – it’s just not quite as high as 304 stainless steel. Also, be aware that the absence of nickel can make 430 stainless steel vulnerable to cracks during pressing.
430 stainless steel does have good thermal conductivity, which helps in applications where heat dissipation is important. It also has slightly higher heat resistance compared to 304 stainless steel.
Unlike 304 stainless steel, 430 is magnetic – hence, why it’s ideal for magnetic catches, as seen here. Like 304, 430 stainless steel also has good formability. However, ultimately 304 stainless steel has more versatility in its applications, hence why it's the most widely used of all stainless steels.
What is 430 stainless steel used for?
430 stainless steel costs far less than 304 stainless steel, which comes down to grade 430’s lack of nickel. While the price of metals constantly fluctuates, it’s not unusual to see grade 430 cost anywhere between 55% and 75% of 304 stainless steel.
304 vs. 430 stainless steel uses have some overlap. Common applications for 430 stainless steel include the following:
| Industry | Typical application | Why |
|---|---|---|
| Automotive | Mufflers, trim | Corrosion resistance properties |
| Aircraft | Compressor blades | Corrosion resistance properties |
| Energy/power generation | Turbine engines | Corrosion resistant, maintains strength in heat |
| Consumer appliances | Refrigerator cabinet panels, range hoods, dishwasher linings | Cost effectiveness, easy to clean |
| HVACs | Heat exchangers, furnace parts | Thermal conductivity, Resistance to corrosion |
| Components | Fasteners/screws, Worm-drive hose clamp | Ease of fabrication, Resistance to corrosion |
Properties of 430 stainless steel
304 vs. 430 stainless steel properties, or rather, 304 vs. 430 appearance: Both have aesthetic appeal. Grade 430 has excellent finish properties, and coupled with its costs, it explains why it’s also used for decorative purposes, such as in elements of architecture and jewellery
304 vs. 430 stainless steel: a comparison
It helps to see the composition of these stainless steel. As you can see, they’re similar in many ways, but the lack of nickel in grade 430 is their main difference.
| Element | 304 stainless steel % | 430 stainless steel % |
|---|---|---|
| Carbon | 0.07 | 0.08 |
| Chromium | 18.0 – 19.5 | 16 – 18 |
| Nickel | 8.0 – 10.5 | - |
| Silicon | 1.00 | 1.00 |
| Manganese | 2.00 | 1.00 |
| Phosphorous | 0.045 | 0.045 |
| Sulphur | 0.015 | 0.015 |
| Nitrogen | 0.10 | - |
304 vs. 430 stainless steel strength
Grade 430 contains slightly more carbon, which means it should be stronger than 304. That said, the nickel in grade 304 contributes to its strength. Here’s how they’re mechanical properties compare – note, the ultimate tensile and tensile yield strengths measure the materials’ resilience to tensile (pulling) forces. The yield strength reflects the maximum stress before the material will deform permanently. The ultimate tensile strength describes maximum stress before fracture.
To understand the Rockwell B hardness test, see our guide, What’s shore hardness and why should you care?
| Properties | 304 stainless steel | 430 stainless steel |
|---|---|---|
| Ultimate Tensile Strength | 505 MPa | 517 MPa |
| Tensile Yield Strength | 215 MPa | 345 MPa |
| Hardness (Rockwell B) | 70 | 85 |
| Elongation at Break | 70% | 25% |
304 vs. 430 stainless steel differences
In summary, these are the primary characteristics of both steels:
| Characteristics | 304 stainless steel | 430 stainless steel |
|---|---|---|
| Corrosion resistance | Excellent | Very high |
| Magnetic | No | Yes |
| Weldability | High | Limited |
| Hardens during cold forming | Yes | No |
| Formability | Very good | Good |
| Machinability (annealed) | Fair | Good |
| Resistance to elevated temperatures | High | High |
| Maximum intermittent service temperature | 850°C | 850°C |
Download free CADs and try before you buy
Free CADs are available for most solutions, which you can download. You can also request free samples to make sure you’ve chosen the right product for what you need. If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.
Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.
Questions?
Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.